Hi Experts,
I am seeing through an osciloscope a ripple on the DC level in the Vout pin of my REF102 device and this is affecting my circuit performance, the Vpp of the ripple is around 15uV over the 10V DC signal, and it has a frequency of 0.16 Hz... Please refer to the circuit attached, I removed C8 and C9 and instale a 0 ohm resistor on R3 to see if capacitance load was affecting but still seeing that ripple... Could anyone help figure out the rootcase of that ripple? Thanks!!