Other Parts Discussed in Thread: EV2400, BQ40Z50
Hi all,
My customer is using BQ40Z50-R2 in their system, and is seeing the following behavior from their battery pack:
1. They discharge the battery to 0% SOC
2. The device enters undervoltage protection mode
3. When system power is applied, the BQ40Z50-R2 does not broadcast SMBUS data to the battery charger
4. The customer must connect to the EV2400 and wake up the gauge
5. Customer trickle chargers the battery until V+ hits 15V, then the BQ40Z50 wakes up and starts broadcasting to the system battery charge and charging at the normal 1/10 C charge current.
The customer wanted to know if there is a way to configure the gauge to either wake up and begin broadcast normal charging instructions with out the trickle charge, or if there is a recommended method to tell the system that the BQ40Z50-R2 is about to go in protection mode and have the system shutdown. Could the BTP function be used here? If so, is there a way to determine the optimal DoD/SOC to toggle the BTP?
Thank you,
Jon