Hello,
I designed a dcdc converter board designed to pulse power a set of high power LEDs.
I have 4 LM5118 Circuits which charge up a 1200uF capacitor which is then switched on across a LED providing a 11A,52.5V pulse at 3.7% Duty.
This works great when I have a single LED driver activated and a single LED being flashed. In this state the DCDC driver consumes 580mA at 48V to power the capacitor. This translates to an efficiency of (52.5*11*.037)/(0.550*48)=80%efficiency (which is not the best but I think I can improve it by using capacitors with a much smaller gate capacitance).
However, when I power up multiple drivers and LEDs in parallel the efficiency drops dramatically. I end up having the same output power on each led but at 3.3A at 48V input. This translates to an efficiency of (4*52.5*11*.037)/(3.3*48)=53%effsiciency
I suspect this may be an issue with the synchronization of the supplies through the SYNC pin, however when I detach this pin, the entire converter starts shorting out. Both mosfets open and let power flow freely through the inductor.
I am at a lose, please let me know if you have any ideas whats going on.
Best,
-Danny