This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63806: Shutdown quiescent current

Part Number: TPS63806


Hi,

In our application, TPS63086 is selected to meet requirements below, at the moment, is it the best PN?

1, Input: 3.3V - 3.8V (Li-Ion rechargeable battery).

2, Output: 3.8V (typical), maximum 400mv voltage drop for load 2A pulse current.

Also, what's the quiescent current in shut down mode? Thanks.

Regards,

Ma Dawei