This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24230: without battery issue

Part Number: BQ24230
Other Parts Discussed in Thread: CC2642R

We have two module for BQ24230 application , one is with battery and the other is non-battery .

With battery, our system boot fine. 

But without battery condition, our system boot failed ..Do the BQ24230  support only Vin from 5V ? Or I need to do something... (TS pin is pull down with 10K ohm)

(