This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ULN2803A
In one of our new design we are using ULN2803A for driving Relay. Circuit is as given in attachment.
Please confirm whether PULL DOWN is required an Pin1 of ULN2803. And also confirm whether schematic is correct.
Thanks in advance.
Hi Haranath,
I do not think the resistor R75 is needed as COM can be directly pulled to 5V.
There is no internal pull down or pull up for the IN pins so depending on your GPIO behavior, a pull down or pull up is necessary.