This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

REF5045A-Q1: REF5045A-Q1

Part Number: REF5045A-Q1

Input voltage range of the REF5045A-Q1  

Hello, 

I am planning to use REF5045A-Q1 to obtain low drift and precise voltage which will be the control voltage of my oscillator (VCOCXO). I have some questions about its input voltage range. In the product datasheet, under the section of 7.5 input voltage range is given as  VIN = (VOUT + 0.2 V) to 18 V. 

1. As indicated in the datasheet, when we look "Figure 10. Quiescent Current vs Input Voltage" graph, it is shown that  IQ current is not altering (mostly stable at 25 °C) between the voltage range of 5-18V. Does it mean that if I supply 9V to the input pin, Vin (pin 2),  will REF5045A-Q1 still yield 4.5V  as given in the datasheet? 


2. Or Can I supply any voltage in between VIN = (VOUT + 0.2 V) to 18 V?

3. Or is there any nominal input voltage that has to be given as an input voltage (to Pin 2) for REF5045A-Q1 to yield a 4.5 V output? 


Thank you in advance, 

Huriye ÖZDEMİR.