This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello team,
Hope you are doing well. Customer is using LM46000A-Q1 in their design and tested the part for 1KV/-1KV. The part did not pass as per the ratings in table 6.2 ESD ratings. Customer is asking if we can verify this device will pass IEC61000-4-5 surge test that is 500V/-500V.
Regards,
Randhir
Hi Kalsi:
Do you know how customer test the ESD when it works or not work ,which function failued?
is it failued in HBM test?
Daniel,
See customer response below:
Hi Kalsi:
ESD rating is different from surge test, the energy is different. for Suger test, customer need add extenral protection compoent like TVS to make sure that the no pin is out of its max votalge rating
Thanks