This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

which one is more appropriate?

Other Parts Discussed in Thread: BQ2014, BQ2004, BQ2005, BQ2060A

We have to upgrade a  product very shortly. This used  1 of Bq2004 &  1 only Bq2014

New design will have 2x BQ2005 & surely 4 BQxxxxx gas-gauge

I am divided between: Bq2014 or Bq2060A.

2060A has 60 pages to digest & seems quitea bit involved. It needs EEPROMs etc.

2014 is straight forward.

Client is right to wonder why change to 2060 when 2014 has been working so well for all these years? With the burden of having to program during manufacture.

Technically: which is more apprpriate to  use now in a new design?

-robin