This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3423: Please help to check if lm3423 schematic is correct

Part Number: LM3423

1. Pull down the lm3423 stick up pressure, it can't rise, abnormal (15V to 19v, pull down the lm3423 stick up pressure to 15V, it can rise to 19v if it doesn't stick up normally).

2. The LED is not on. The LED VIN and led GND of J7311 are the voltage boosted from the front end (both led VIN and led GND are the same voltage).

CRE-C2-MT8163-V1.0 99.sch

3. The drawings are made according to your reference design (output: 8 LEDs at 2.5A), and our LED drawings are also attached. Please help to check where to modify, thank you!CRE-C2-MT8163-V1.pdf创荣3.5寸项目LED灯框图.pdf