Other Parts Discussed in Thread: , BQ76920, BQ76930
Hi
BQ78350 is not recommended now.
It can be replaced by BQ78350-R1 but it is not functionally equivalent.
What is a point to be careful when we change BQ78350 to BQ78350-R1?
BestRegards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Na Na,
The BQ78350 had some behaviors which were not as desired, and BQ78350-R1 was prepared. There was not a migration document prepared to describe changing from BQ78350 to BQ78350-R1. Generally a person might think the -R1 is how the part should have worked, but there are some added features, so it is different. It is hard to say what is most important to your implementation since concerns vary.
To understand the differences, see the ReleaseNotes.txt with the -R1 device firmware http://www.ti.com/lit/zip/sluc594 . For details compare the feature description in the technical reference manuals for the BQ78350 (http://www.ti.com/lit/pdf/sluuan7 ) and BQ78350-R1 (http://www.ti.com/lit/pdf/sluubd3 )