Hi,
My application uses Nokia E61i (lithium ion) battery with a capacity of 3000mAh.
I am in lookout for a battery gauge chip that can implemented inside the system and not embedded in the battery pack.
I need to determine the residual capacity of the battery. The important point is that I am not online charging the battery in our system , but charge it offline in a remote location and reinsert the recharged battery to the system. i guess Coulomb count technique may not work in this scenario. May be the prediction may not be very precise but an approximate judgment would do.
Can battery gauge chips sense the capacity with a reasonable degree of accuracy in this condition??
Which chip will be suitable for this removable battery pack application??
Thanks in advance for your key inputs.