Other Parts Discussed in Thread: UCC21530, , UCC21222
Hello,
I have one doubt regarding the dead-time pin functionality of UCC21520/UCC21530. When the pin is left open, the dead-time is set to <15ns.
It is not clear from the datasheet if overlap protection is active or not in this case.
Looking to the board manual, this is also not clear since for this situation the 2 PWMs shown are complementary switching.
Checking the other datasheets for confirmation, I found out that in the 150mil DSO UCC21522 there is the following statement:
"Tying DT to VCCI or leaving DT open allows the outputs to overlap."
For DTC left open, the overlap protection seems to be deactivated for UCC21522. What about the other drivers in 300mil DSO and LGA (as UCC5120 in 300mil DSO and LGA options)?
Is the approach different between packages?
Best regards,
Luca