This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24650: the design of a charger

Part Number: BQ24650
Other Parts Discussed in Thread: BQ24610

Dear Sir:

       I  want to design a charger to charge the 2S battery. The max voltage is 8.4V and the max current is 8A .Can I use the  bq24650? Or should I use another chip ,eg ,the bq24610?

       Which chip fit to the design?