Other Parts Discussed in Thread: TPS2549
Hi Emma
I have few questions to ask about TPS2546 configurations.
Below is the application scenario on the USB port
#1. Supports USB thumb driver and HDD for data transfer
#2. Supports various mobile phones for charging only mode. No data is required
Questions
1. Does below mode best suit for the applications such as
SDP/CDP Auto Switch for #1
DCP auto for #2
2. If only configure SDP/CDP Auto Switch for #2. What happened to the phone’s charging condition? Would it work similar as DCP auto?
3. Since there is no SDP/CDP - DCP Auto switch mode, user has to perform software setting that depends on what portable USB device is inserted. Is there any detection that could assist to inform MCU to decide which mode to configure? Eg. When thumb drive / HDD is connected, it selects SDP/CDP and if a phone is connected, it switch to CDP Auto.
4. Do you have the phone compatible list supported by this device with DCP auto?
5. Do you have the feature comparison of TPS2546 vs TPS2549 ? Cable compensation is not required here. Does it make sense to use newer TPS2549?
Rgds
Kelvin