Part Number: TPS22913
Hi, TI team,
There is a project which uses TPS22913. The desing circuit is as below:
1. Due to the EN is low, although the 5VDD is ready, the 5VDD can't be built at the network of "5VOUT";
2. And then the EN_LDO is high, and the 3.3V is built at the network of "5VOUT";
3. SET EN to be high level, and the 5VDD will pass through TPS22913, and the 5VDD will be built at the network of "5VOUT";
Please help check the operation principle is right or wrong!!!
I found that there is a MOSFET QOD on the datasheet.
If the EN is low level, the VOUT pin will be pulled to ground or not?
If VOUT is pulled to ground, the TPS22913 will be burnt if VOUT is with external LDO as above. Right?
Thanks very much!
BR
Eleven