This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ20Z95 & CHIPSET US15W compatibility



Dear,

I am currently testing a kontron motherboard equipped with an Intel US15W chipset.
This card is power supplied with a Inspired Energy battery which is controlled by a BQ 20Z95.
I receive SMBUS informations with many mistakes, or I do not get at all. (and the battery is indicated as "not present" in the motherboard bios)
 
 1. I wanted to know if this problem was known (incompatibility US15W BQ 20Z95) ?
 2. Is there any problem of compatibility between US15W & BQ 20Z95 because the chipset is SMBUS 1.0 compliant and the BQ 20Z95 is 1.1 compliant?
 2. If yes there is there a solution for this?

For information :
- I have tested with several batteries and several motherboard it is the same.
- When I connect a SMBUS charger with the battery and the motherboard, the battery is indicated as "present" in the motherboard bios and I have less mistakes.
- The motherboard is a nanoETX-SP from kontron (SMBUS 1.0 colmpliant)
- Battery is a NI2020 from Inspired Energy (SMBUS 1.1 colmpliant)
- Charger is an EB259 from Inspired Energy (SMBUS 1.0 colmpliant)


 Thank you in advance for your help