This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24193: What is the expected VSYS when the battery is disconnected?

Part Number: BQ24193

Hi,

There are situations in the project where the battery may get physically disconnected. The datasheet explains how VSYS behaves as a function of VBAT, but I have not understood from the given description what VSYS voltage to expect if the battery is disconnected. What value should I expect?

Also, VSYS is described to track 150 mV above VBAT when not charging. VBAT can be set to charge up to 4.4V, yet the maximum VSYS range is stated as 4.35V. How should that be understood? What VSYS voltage should I expect when not charging if the charging voltage is set to for instance 4.35V or 4.4V?

Thanks!