Tool/software: WEBENCH® Design Tools
Hi, I'm using LM61460-Q1 in a design as a regulator for charging a 12V lead acid battery from a solar panel. ( I also have a VHF receiver on the board and that is why I chose this IC because of low radiated EMI.)
When the battery is absorbing the panels full capacity, up to 5A, the IC will be in drop out, ie not reaching the regulating voltage (14.4V). Once the battery reaches 14.4V the IC will begin to regulate and the current will progressively drop while the panel's voltage, ie Vin, will begin to rise towards 18V or 19V. After a while the feedback voltage divider will be adjusted (n-fet closes removing a resistance in parallel with feedback voltage divider's bottom resistor) to reduce the regulating voltage to 13.6V. Iout may drop to very low levels, say 0.1A, while Vin will rise close to the panel's open circuit voltage of 20V.
I don't need a rapid transient response, just stability. When I adjust the input parameters in Webench sometimes it shows series RC (1K and 10pf) in parallel with the feedback dividers top resistor. What would be
the best values for stability when regulating at 14.4 or 13.6 with Vin up to 20V and low load?
If I enter I-out max of less than 0.5A, Webench says "Design update failed. This design is not stable due phase margin either smaller than 35 or greater than 120"
This is a bit of a worry considering once the battery has charged and the IC is regulating, Iout will drop to levels well below 0.5A. I didn't notice a minimum load requirement mentioned in the data sheet.