Other Parts Discussed in Thread: UCC28951
Hi Expert,
We see the UCC28950 miss switching cycles occasionally from half load to full load.It cause the system level failure.
Pls see the major parameters and project information:
Applicant : PSU
Output power :1000W
Vo:12V
Issue waveforms:Pls see attachment
Key parameter of design:
--Transformer ratio: 47T:2T:2T
--60KHz switching Frequency
Now the issue can be avoided from change the Tmin from 130K to 30k.The engineer want to know the root cause and concern if had.
Pls help to clarify:
1) Why change the Tmin from 130K to 30k can solve the switching cycles missing
2) Can parallel a small cap on Tmin pin for noise immunity improvement
3) To charge the Tmin from 130K to 30k can help the noise immunity
4) Can TI share detail Block Diagram to know the Tmin behavior
5) Any suggested solution to slove miss switching cycles occasionally if Tmin from 130K to 30k is not preferred.
Best regards,
Eric Lai
Field Application Engineer
Texas Instruments Taiwan Limited
O: +886-2-2175-2582
M: +886-909-262-582
E-Mail:Eric.Lai@ti.com UCC28950 miss switching cycles Issue.docx