Other Parts Discussed in Thread: LMR33630
Hi Team,
Some customers report that the LMR33630 has exceeded the junction temperature of the IC when the input is 18V, the output is 3.3V, 2A, and the ambient temperature is 80 ° C.
Then the value in the data sheet is 72.5 ° C / W, which seems to be really high. Is there any reason to avoid this?
Best regards,
Ansel