Hello Sir,
The bq20z655-R1 datasheet recommended to use 5-mΩ to 20-mΩ typical sense resistor on page 14.
The original text is as follows ,
The bq20z655-R1 uses the SRP and SRN inputs to measure and calculate the battery charge and discharge
current using a 5-mΩ to 20-mΩ typical sense resistor.
In our battery pack design , we choose 2mΩ for sensen resistor . I want to kown , What will happens if we choose the sense resistor is outside of 5-mΩ to 20-mΩ ?
When our system power on ,the inrush current is over 50A . So we need choose the lower sense resistor than the 5 mΩ for bigger current sense.
Thanks!
Billy