Hi
We would like to design VSTART=5.5V and VSTOP=5.0V
after calculation we get R10 =167K, R11=47.2K and our schematics as below.
However, using the above R10 and R11 value to do real test we see VSTART=6.33V and VSTOP=5.2V. this is different from our calculation result.
Would you help review anything wrong with our schematics below ?
Also is it required that Vin need to be > Vout + 2V ?