This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2660: surge and burst test

Part Number: TPS2660
Other Parts Discussed in Thread: TPS2663

Hello team,

I am looking for devices that protect boards operating in an industrial environment (19Vdc: 29Vdc) from under voltage and over voltage. I noticed TPS2660x and TPS2662x. The boards where these will be used need to comply with Surge and Burst tests IEC 61000-4-5 and IEC61000-4-4; between the two devices it seems that only the TPS2662x is able to pass both, is it true?

In case you know of any other device, could you please let me know?

Thank you in advance for the support.

Best regards,

Adrian