This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61087: Compensation network calculation

Part Number: TPS61087


Hello,

I am designing a boost converter based on TPS61087, powered from a single Li-ion cell. Output voltage is 16V at maximum 300mA. The load will be a PWM'd motor.

The formulas for compensation network presented in the datasheet are a bit unclear to me.

Inserting the formula in Mathcad, yelds he following results:

Using 110 without a unit yelds the wrong units for R_comp and C_comp.

My question is what does the 110 and 7.5 values represent and what are their units?