This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25890: PMID short circuit protection with VBUS in

Part Number: BQ25890

Hi Team,

Does BQ25890 have PMID short protection with VBUS in? If not, what would happen if it pull too much current(>3.2A) and how should we protect it?

Thanks and Best Regards,

Will

  • Will, 

    Pls refer to the internal block diagram on the BQ25890 datasheet, the internal FET Q1 has a body diode. There is no current limit from VBUS to PMID. You have to add external circuit for the protection of high current from VBUS if PMID is short to GND.