Hi according ot he Datasheet the LM3881 will during power up show a short pulse at the FLAG1-3 outputs because I assume the outputs follow the Vin independent on what EN PIN is telling. IS this correct?
How can this be addressed if the device which should be controlled by the LM3881 is powered before the LM3881 and therefore the 0.65Volt could unintentionally be enable by the 0.65Volt pulse?
If there is a cap connected to the EN-PIN would the pulse at power up still occure?