Hello,
I want to use the TPS5430 (24VDC input to 5V output) parallel to a second power supply 24VDC input to 5V output. in some applications the TPS5430 has to be disabled, in this case I will have 24VDC @ the input of TPS5430, ENA pin below 0.5V and 5V at the output of TPS5430 from the second power supply.
my question: is it allowed to use the TPS5430 under the above conditions?