Hello,
We have implemented TPS23756 into our Wifi access point product which uses POE or external power from 12V to 48V. Whenever voltages is around 24V or 48V using adaptor, the TPS23756 (or its whole circuit including transformer, inductors or caps), there is a very low volume audible ringing occurring when the access point has started up during booting. After booting, around 1 minute, the noise disappeared.
Can anyone suggest what I can try to debug this issue?
Thanks
Duncan