This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2832: Thermal Resistance

Part Number: TPS2832


Hi,

The Theta J-A & Theta J-C parameters of TPS2832 is not available in the datasheet. Could you share the same?

Regards,

Veerasamy

  • Hello Veerasamy,

    The junction to ambient thermal resistance can be determined from the  dissipation rating table on page 4 of the datasheet. The power rating is 330mW at ambient temperature of 70 deg C and 240mW at ambient of 85 deg C. With the recommended junction temperature of 125 deg maximum, with 330mW and a temperature difference of 125-70 deg C (55 deg C), there is 55 degC rise/330mW or 167 deg C/W. This same result is found with the 240mW and 85 deg ambient rating.

    Confirm if this addresses your questions, or you can post additional questions on this thread.

    Regards,

  • Hi,

    Thanks for the confirmation. This addressed my query.

    Regards,

    Veerasamy