This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Boost converter with zero current off state and still have a flexible startup

Other Parts Discussed in Thread: TPS61023, TPS61022

Hi,

Could you please recommend a boost converter that has a zero current off state and still have a flexible startup.

For example, a BLE temperature sensor device. Its power source is a primary cell battery Li-socl2 3.6V, that powers up the rest of the system and I need a boost converter that is used to regulate the output voltage to power up the sensor that requires 5V supply, which has no current leakage when the temperature sensor is not in use. 

Thank you.