Part Number: BQ35100
Hi All,
There are no description about Scaled impedance named "Scaled R" parameter, can you provide this description corresponding ?
What is the functionality difference "Scaled R" and "Measured Z" parameter ?
BR,
Loïc
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: BQ35100
Hi All,
There are no description about Scaled impedance named "Scaled R" parameter, can you provide this description corresponding ?
What is the functionality difference "Scaled R" and "Measured Z" parameter ?
BR,
Loïc
The gauge has a built in impedance data for a reference cell that has a different absolute impedance than the actual cell (e.g. different capacity cells with similar/same chemistry will have the same relative impedance profile but different absolute impedance as a function of DOD).
The gauging algorithm will calculate a scaling factor when a fully charged fresh cell is connected by measuring impedance and comparing that to the reference impedance that is stored inside the gauge.
Doninik,
When you talk about the reference impedance that is stored inside the gauge, do you refer to chemistry programmed in the gauge ?
So the scaled R is completed by the Gauge, we don't must write it ?
What is the difference bettween ScaledR(): 0x16/0x17 and MeasuredZ(): 0x22/0x23 value ?
BR,
Loïc
Yes, the reference impedance is part of the chemistry data.
>So the scaled R is completed by the Gauge, we don't must write it ?
No, you don't have to write it.
>What is the difference bettween ScaledR(): 0x16/0x17 and MeasuredZ(): 0x22/0x23 value ?
The difference is that one is adjusted by the scaling factor as determined by the gauge and the other one is the actual measured resistance.