I need to hook up an aviation headset to HSOL or HSOR. Some aviation headsets have a 10ohm load. According to the TPS65950 datasheet the minimum load impedance for HSOL and HSOR is 14 ohms. Can i just add a 4 ohm resistor to the load impedance to make up the difference? I understand this will cut into the power delivered to the speaker however I'm more concerned about circuit stability.
Danny Nichols