So,
I'm using a tps61500 to drive a string of 1.5A LEDs in serial, I've
implemented a similar circuit using the TPS61500EVM-369 using the
supplied LEDs and a 3v power supply and 3v MCU to provide a PWM signal.
However for the 1.5A LEDs my calculations indicated a 9v or larger
supply for the LED driver necessary. The MCU is still 3v, so should i
use a Voltage Translator to translate the PWM signal to 12v for it to
register on the LED driver? and if so which one would be appropriate?
sincerely
Elliott Johnson