This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC3895: Question for constant current inverter

Part Number: UCC3895

Hello

I will design the constant current inverter using UCC3895

Design Condition:

input voltage: DC 185V

Ouput Current : 10A (RMS)

Can you answer follow question?

1. Is it avalible to adjust frequency by applying external PWM signal to RT, CT terminal?

2. Is it avalible to adjust duty (minimum 5% ~ maximum 45%) by applying MCU signal to EAP terminal?

3. What happens to switching operation (duty or phase shift ) if current is consumed below that in constant current 10A?

Best regards