Please help confirm TPS25221DBVR Output continuous current is 2A or 2720T(NOM) 2850 (MAX) at RILIM = 20 kΩ ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Kevin,
The recommended max output continuous current is 2A. Meaning as normal work, suggested to load not above 2A.
RILIM = 20 kΩ means the setting current limit is 2.72A(typical). Meaning as with heavy load or short circuit, the switch will limit the current to 2.72A.
For TI's policy, I will first click resolved button.
If you have any other concern, contact me any time.
If you think resolved, please help click 'Issue is solved button'.
Thanks.