This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28C42: Can I use this part for 50VDC-300VDC to 14VDC/6A non-isolated converter design

Part Number: UCC28C42
Other Parts Discussed in Thread: TPS2838

Hi,

I am looking for a converter design with the input of 50VDC-300VDC and output is 14VDC/6A. No isolation requirement. 

Can I use UCC28C42 along with synchronous driver IC TPS2838?. UCC28C42 and TPS2838 are powered separately using a buck converter UCC28880DR (50-300VDC input to 14V/100mA).

Please see the below diagram for reference.

Else, can you please suggest a solution for my requirement. I don't use fly back topology as there is a customized transformer involved. 

Regards,

Ajmal