I am planning to build a 10 W active clamp forward converter using GaN FETs instead of conventional Si MOSFETs. I came to know that there are no dedicated Forward controller drivers for GaN devices, Kindly suggest me a combination of modulator and driver I should use for my purpose . GaN device that I have been planning to use is is nearly of 200V and 5A. So, it would be a favor if you could suggest a device with compatible modulator and driver combination.