Other Parts Discussed in Thread: BQ78350-R1
Hello,
I have 2 questions regarding the CEDV gas gauge calibration:
1. How are 0% and 100% SOC defined by the algorithm? I assume that the configuration file parameter "CellTermV" will determine 0% SOC, is this correct? Will the algorithm assume that the battery is at 100% SOC at the beginning of each continues discharge test?
2. To my understanding the chip can take up to 3 external thermistor measurements. Which of these signals will be used for the calculation of the gas gauge? Or will an average be used? I'd like to know in order to determine which data to use for the temperature columns of the configuration file.
Thank you.