Other Parts Discussed in Thread: BQ34Z100
Hello,
I'm monitoring two batteries with the BQ34Z100-G1, I need to switch the batteries in specified moments.
I'm facing a refresh problem with the SOC after I switch one battery (the batteries are the same model), but only when the SOC of the battery that is replaced is higher than the new one.
For example: BAT1_old SOC = 90% switched with BAT1_new SOC = 60%.
The value of the SOC stays at 90%, even when the battery is discharging.
This a problem related to the algorithm used to calculate the SoC or is a problem of programming?
Best regards,
Andres Suarez