Other Parts Discussed in Thread: TINA-TI
Hi!
My customer wants to use Webench to deisgn with TP54320
These are his parameters:
VIN 10.8-13.2V
Vout 3.3 and 5V 3% acurancy
Iout 1.5A for 5V rail and 2A for 3.3V rail
I have set frequency at 700kHz getting inductors 10uH for 5V power supply and 6.8uH for 3V3 power supply. Both designs are X7R only and so far I do have these two type used for input and output buffer. Inductors are from IHLP2525 series.
why I am not able to see the old menu and recompensate the circuit for example TPS54320?
The customer also tried Power Stage designer, but needs help.
Kind regards,
Marion