This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5180-Q1: LM5180 power supply synchronization & Simplest way to generate the gate driver power supply

Part Number: LM5180-Q1
Other Parts Discussed in Thread: LM5180

Hello ,

I am using  LM5180 for generating IGBT gate driver power supply(+15 and -8V),since it is 3 phase inverter i am using six LM5180 (3 for high side and 3 for lowside).

How to synchronize all the six power supply so that i can add only single EMI filter at the power supply input entry?if not possible suggest me suitable method to generate gate driver power supply?(it should be cost effective)

Application :HVEV

Input range=9V-16V

Output:15V and -8V ,0.15A

Reagrds,

Bhupathi