This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ20Z655-R1: Update the chemistry table on BQ Evaluation Software(Version 0.9.80)

Part Number: BQ20Z655-R1
Other Parts Discussed in Thread: BQEVSW

Dear Sir ,

Our supplier used BQ20z655-R1 to design 4s2P battery pack. The cell is chose Panasonic: UR18650NSX (2600mAh) ,but the supplier use chem ID is 2068 ,because 2068 is reference from TI .

I down load the chemistry selection table form TI website  and i can see our cell Panasonic: UR18650NSX (2600mAh) chemistry ID is 2067.

I could't find chem ID 2068 in the cell chemical ID list on BQ Evaluation Software(Version 0.9.80). 

The chemistry select table only can support 0100 to 0800.

Clould you help to provide the  chemistry ID is 2067  and 2068 for me to update chemistry table on BQ Evaluation Software(Version 0.9.80)?

Thanks!