This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

High Volt and Current DC power supply

I've a requirement of DC regulated power supply of following specifications .

Input : 3 Phase AC Supply(220-220-220-0) , @ 50Hz.

Output Voltage : 120 VDC.

Output Current : 30 Amps.

The load may be inductive load.

Pls. help me to design the Power Supply .