Part Number: BQ34Z100-G1
Other Parts Discussed in Thread: BQSTUDIO,
Hi,
When I tested my board with a fresh part soldered, BQSTUDIO (Ver 1.3.86) can automatically detect my part bQ34z100G1 with 0100_0_16, Addr 0xAA (under the DashBoard)
However, if I hit the "FW_VERSION" in the command tab, the next time I boot up, the part isn't recognised in the target selection window as the autodetected device is 0000_0_00. I have the manually select 0100_0_16-bq34z100G1 device and receive a warning that the detected part is not compatible with this application. Once I do this, I am able to connect with the device but in the dashboard the device now reads bq34z100G1 with 0000_0_00, Addr 0xAA.
Reprogramming the part with a new firmware does not revert the firmware version back to 0100_0_16.
How do I ensure that the firmware is properly programmed?
With kind regards,
TzeWei