This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2663: OVP function question

Part Number: TPS2663

Hi Team,

Would you advise that

Looking at the evaluation board 26630 side,
Current LIMT setting: 6A
Load current: 5A
 
UVLO operation is OFF by swinging the voltage to the lower limit for 18V. Returning to the upper limit and confirming ON, there was no problem.
With OVP operation, turn the voltage to the upper limit for 33V and turn it off. Return to the lower limit and do not turn ON.
Looking at the operating status, it seems that it has once returned to ON, but it seems that overcurrent OFF is operating.
If the load current is lowered to 3A, operation will be possible.
I also checked the flowing current, but it didn't look like an abnormal current was flowing.
Is this correct behavior?
Thanks
Best regards,
Shidara