Other Parts Discussed in Thread: PMP10748
Hi TI experts,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI experts,
Hi Buta,
Thanks for reaching out!
LM5060 can work for OVLO, UVLO, inrush, reverse polarity protection. It is also able to drive multiple parallel MOSFETs but it does NOT act as ideal diodes OR-ing means LM5060 provides reverse current protection only when it is in OFF state.
You would need LM74700 for ORing and LM5060 to act as controlled switch. Please also reach me via email to share other options.
Best Regards, Rakesh
Hi Rakesh,
Thank you for your reply.
I want to clarify the requirement 3:
3. act as switch controlled by external signal so it will disconnect _an individual_ battery from the load.
I check out the ref design PMP10748 Complete Front End Automotive Reverse Polarity and Series Fault Protection Reference Design, it seems it could not disconnect one of the batteries from the load. Do you have any suggestion or ref design?
Best Regards.