Hi
Customer feedback the quiescent current is too big in light load mode.
Vin: 12V, current:17mA
Vout: 5V, loading is 5V/4mA
Switching frequency is 2,1MHz
As we can see from below curve, the efficiency is around 85% in 12Vin/5Vout/4mA condition.
5Vout*4mA=0.002W/85%=0.023W_pin/12Vin=0.0019A (1.9mA) but customer get 17mA on Vin.
so that is make sense?