Other Parts Discussed in Thread: TPS54160
Hi,
Currently i'm doing the experiment 1 test 1, Vin 24V, Vout 3.3V, Iout change from 0.1A to 1.5A.
i find when the Iout is lower than 0.7A, the Vsw will show some weird waveform. shown below.
Iout=0.1A
Iout=0.5A
In the Iout=0.1A image, i think maybe TPS54160 is in ECO-mode. But what cause the ringing in the red circle?
In the Iout=0.5A image, what cause the Vsw is high in the red circle?
Thanks.
Best regards
Mason Liu