Other Parts Discussed in Thread: TPS63050, BQ24195L, BQ25606, BQ25601
Hello,
I'm looking for an charger IC which provides my system side with 3.3V (max 0.5A needed).
Device should be charged from single Input USB/ High Voltage Adapters, Input Voltage 5 - 13.5-V.
Battery INR18650 (or similar type):
LiNiCoAlO2, 3300mAh, max charge current 2000mA
Fuel Gauge and Protection(recommended from last post):
Single Cell Li-Ion Battery Fuel Gauge With Integrated Protection bq27742-G1
I cant find any charger IC which has an system output with 3.3V for powering my Microcontroller.
I want to use a I2C interface to communicate between Hosts an IC's.
Do I need to use a non-power path charger (linear regulator or switching converter) with an external buck converter instead? (For example TPS63050)
Would be happy if someone can give me an advice.
Greetings
Florian Mayerle